Part Number: TPS54302
Hi there.
I have a question about using the TPS54302 step-down converter with light loads.
In my design I was originally using the TPS6217 (up to 500mA) wich was okay for my circuit (not tested, just designing schematics and PCB). But chip is out of stock in DigiKey and it's expensive on China market so I wanted to change it.
The main thing about the TPS54302 model is that under 500mA loads enters in Eco-mode (pulse skipping) and I'm not sure about it's consequences.
I have a design wich consumes 150mA top. The step down converter will mainly use to power a 5V sensor and as a Vin for 3.3 linear regulator (MCP1702).
The regulator powers MSP430FG6047 uC and other things.
Could I expect problems by using the TPS54302 continusly in pulse skipping mode? The idea it's to power the all system with 12V and 24V. The converter fix an 5V output and then the regulator a 3.3V.
Will the 3.3V linear regulator function properly?
Any tip or comment about this would be appreciated.
Thank you!!