This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594-Q1: Simplis Multiphase Error

Part Number: TPS6594-Q1

Hi Team,

I'm having trouble with the TPS6594 simplis AC Transient model whenever I change phasecount to more than one I get the following error:


Unable to locate the definition
of 'subcircuit SIMPLIS_DIGI1_D_MUX_YX$U2$333' in the
input, include, or library file(s).

I get this with both the 4.4MHz_MP setting and 2.2MHz_MP setting. I downloaded the model straight from Ti.com. I'm also using Simplis version 8.3.

Any recommendations how how to get more than one phase to work?

Best,

David