Part Number: TPS650864
Other Parts Discussed in Thread: TPS650861
Hi,
I would like to understand further on the CTL pins for the bootup sequence in TPS65086401.
FPGA device to be powered is Xilinx Zynq Ultrascale+ ZU3CG.
The power up sequence is described in Figure 8-7 of the TPS650864 datasheet.
- So should only the CTL1, CTL6 and CTL4 pulled up to 1.8V rail?
- CTL3 = 1 (pull up to 1.8V), CTL2 = 0 (pull down to GND) for BUCK6 output = 1.2V?
- This 1.8V rail should be available in the system before all the outputs from the PMIC are enabled?
- Or should there be any control sequence of external signals connecting to CTL1/6/4 pins to enable the power up sequence stated in Figure 8-7?
- If not used, for example CTL4, they should be pulled to GND? In this case, will BUCK3, LDOA3, SWB1_2 and BUCK5 enabled?
- If CTl1 is pulled to GND, does it mean all the subsequent power up sequence of PMIC outputs will all be disabled (except for LDO5 and LDO3P3)?
Regards,