Other Parts Discussed in Thread: BQ25792, TPS25750,
Hello,
I have an application that has 2x 18650 batteries (7.4V, 2600mAH) and need to charge them from USB adapter.
My client wants to use a USB type-C connector, but we cannot have cost of full USB PD (we considered BQ25792 + TPS25750). For this reason, I'm now planning to use the BQ25886 which will be limited to 15W (5V, 3A), but is much lower cost. Any thoughts on this approach would be appreciated, but isn't the main question I have.
The question I have is how to connect the D+/D- pins of the BQ25886 with USB C. My understanding is that with USB C current limits are set via CC1/CC2 pins, while older USB current limits are set via D+/D-. I also realize that USB C has two pairs of D+/D-, and many USB C connectors are designed for power-only (no data), with just GND, Vbus, and CC1/CC2.
How do you suggest connecting the BQ25866 to a USB C connector for best compatibility? Should I connect the D+/D- pins of the IC to both pairs of D+/D- on USB-C (e.g. is it possible to have legacy adapter requiring the D+/D- negotiation with USB C cable)? Should I also add in the pulldowns on CC1/CC2 in case a USB-C style of adapter is used?
Note that in my design we do not have an MCU and no need for data over USB.
I look forward to any insights you can provide.
Kind Regards,
-Jon