This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122-Q1: multi-phase boost solution

Part Number: LM5122-Q1
Other Parts Discussed in Thread: LM5122, LM5170

Hi

I would like to design multi phase boost application, here is design requirement, 

The boost input voltage is 4.2V~9.6V and output is 12.3V/62A. may I use the LM5122 that configuration is six-phase daisy chain, or any better solution could be use ? Thanks.