Other Parts Discussed in Thread: CSD19534Q5A
Hi
I have a problem with my DC to DC, based on LM5145 TI PWM controller.
Design input voltage is between 36V - 63V (nominal 48V).
Design output voltage is 24V, 4 Amp.
Design PWM frequency is 350 Khz.
When I measure the output voltage, I measure 19V instead of 24V (at no load at all, and at 0.5 ampere load) , the signal at pin 19 (SW), is not stable, it skip cycles, and also the duty cycle at that pin is not stable.
I can hear a small acoustic noise ( like Ashhhh noise, probably comes from the output inductor).
I did the design with the excel simulation tool of TI
Attached the Schematic design, and a scope waveform at pin 19 (SW)
power supply calc.xlsm