This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS76633 Question

Other Parts Discussed in Thread: TLV702

Hello!

I plan to use the TPS76633 in a super ultra low current application (I'm counting the uA) and I have a question: do I need to use an external pull-up resistor on the /EN line or does it already have something inside that will take care of that for me? Even 100K up to 3.3V will bleed 33uA which is ludicrous, compared to the 1uA the LDO consumes when disabled.

Thanks for the help!

Dan