Hi,
I am unable to find conclusive information about this, I would appreciate a clarification if possible.
In my application I have a 5V regulator, and I need to individually distribute/control its output voltage to 4 separate subcircuits. A microcontroller should control the switch(es), but the microntroller is not itself powered by the 5V regulator. Instead, the microcontroller is powered by a separate 3V3 power domain which can and will be powered when the 5V is powered off.
Considering the above, is the TPS22941 tolerant of the the following scenario?
IN = 0V
ON = 3V3
Or must I add some sort of Ioff isolation between the microcontroller and the TPS?
In advance thank you for any help or suggestions.