Can any member of the TPS65073x family source following Vout on DCDC3?
- Condition: TPS65073x running off 1 cell Li-Ion battery
- Vout range: 3.4-3.8V @ 1.5A
- Condition: TPS65073x running off 5V DC supply
- Vout range: 3.4 - 4.2V @ 1.5A
Thanks
-JP
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can any member of the TPS65073x family source following Vout on DCDC3?
Thanks
-JP
Please see the table labeled ordering information on page 2 of any of the TPS6507x datasheets.
Table on page-2 lists default values. The question earlier is referring to the adjustable Vout range for DCDC2 & DCDC3 as listed in tables on page-5 & 6.
The table states that the Vout range can be adjusted with an external resistor divider in the range 0.6 - Vin. Since Vin is connected to the power path SYS pin, the
potential Vout range will depend on the presence of AC/USB power and battery. Please confirm if the TPS65070 can provide the Vout range on DCDC3 as stated in earlier thread.
Thanks,
-JP
The TPS65070 can, by default, supply 1.5A at 3.3V on DCDC2 if DEFDCDC2 = HIGH.
DCDC3 can supply 1.5A at 3.3V by setting DEFDCDC[5:0] = 111111 and by connecting VDCDC3 to VOUT3 or by setting DEFDCDC[7] =1 and connecting an external resistor divider from VOUT3 to VDCDC3. This applies to DCDC1,2,3.
This does not address the question on the upper bound of the Vout range: 0.6 - Vin under the 2 conditions stated in an earlier thread.
-JP
I misread your question. DCDC2,3 of the TPS65070 can supply 1.5A at 3.4V, 3.8V or 4.2V with sufficient AC,USB or BAT when DEFDCDC#[7] =1 and an external resistor divider is connected from VOUT# to VDCDC#; however, this wont be dynamically adjustable.
We don't need the Vout to be on-the-fly adjustable.
What's the voltage drop @ 1.5A in the power path when the device is being powered by either of the following:
- JP
The power path voltage drop is specified in the datasheet for AC (Isys=1A), BAT (Isys=1A) and USB (Isys=500mA and 800mA):