This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24160: default setting

Part Number: BQ24160

Hi, 

What will be the USB input current setting of BQ24160 if:

1) The charger starts from an external DC adapter

2) The charger starts from USB, but without an active device at D+/D-

3) The charger start from USB, but there is already an active device at D+/D-, which does not support BC1.2.

4) The charger starts from an external adapter, but then a valid voltage is applied at USB and the adapter is disconnected.

Best regards, Julia

  • Hi Julia,

    Regarding 1, if connected at IN, default input current limit is 2.5A per datasheet.  

    Regarding 2 and 3, if not detected, default input current limit is 100mA.

    Regarding 4, if SDP was detected, then 100mA.  If CDP/DCP was detected then 1.5A.

    Regards,

    Jeff