This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62230: Searching TI solution for TPS62232 replacement

Part Number: TPS62230


Hi Team,

May I have your help to check if possible to change solution from TPS62232 to the parts listed below to support urgent demands? Yellow marks show that we have stocks for them. 

  • Hello Kygo,

    The closest device to TPS62232 is TPS62235 because both parts have an output voltage of 1.2V. However, TPS62232 has a switching  frequency of 3.0MHz and 2.0MHz for TPS62235. If the customer can change the inductor to 1.0uH, then they can use TPS62235. 

    Below are the key parameters to check if TPS62235 fits the customer application. It is the responsibility of the customer to verify all the application specs if the new device suits their application.

    1. Loop stability (check phase margin)

    2. Efficiency (it should be better due to lower Fsw)

    3. Ripple voltage

    4. Transient response

    Best regards,

    Excel

  • Hello Kygo,

    Just a soft reminder.

    Do you still have further queries on TPS62232 & TPS62235?

    Best regards,

    Excel

  • Hello Kygo,

    If you don't have further queries, I will close the thread. You can re-open it again by posting your comments.

    Thank you.

    Best regards,

    Excel