This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS546C23: Schematic reivew

Part Number: TPS546C23

Dear team

There is a good news that we design in TPS546C23RVFR in customer's new project.

For U10 and U11 are two phase  : Vin=12V,Vo=0.825V,Io=53.53A.

For U49 is one phase  : Vin=12V,Vo=0.8V,Io=18.75A.

Could you help to review the schematic of U10,U11 and U49?

Many thanks

Denny