Other Parts Discussed in Thread: LM2662
Hello Seniors:
Due to my personal design and negligence, the input voltage is positive.
So I can connect the IN of TPS723 to the input GND. Then the input 3.3V is connected to the GND of TPS723? This will work properly?
Because I currently lack a set of negative pressure input. And my circuit boards are all positive pressure.
Is there a faster way to generate a negative pressure to TPS723?
Please also help provide ways to improve.