This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC5350-Q1: Miller clamp feature

Part Number: UCC5350-Q1

Hello,

my customer is currently working on a design and uses UCC5350-Q1 with integrated Miller Clamp as an IGBT driver.

They would like to get more information about the Miller Clamp feature and are particularly interested in:

- when after the switch off is the Miller Clamp active?

- is the MOSFET always switched through on the following picture when the driver is off or only when the clamp voltage is above 2 V?

 

Best Regards,

Stani