Other Parts Discussed in Thread: BQ24192, BQSTUDIO
I have a design using bq27531-g1 battery gauge with bq24192 charger. The learning cycle was run once but the reported capacity was very inaccurate. I collected and submitted data for the chemID selection tool (GPC) and got back a different ChemID than the one initially used. I would like to repeat the learning cycle using the new ChemID, but when I try to follow the instructions in SLUA903 Achieving the Successful Learning Cycle, Update Status does not change to 04.
I am using bqStudio 1.3.101. Initially, Update Status 0 was at 02, which I think is as expected once a learning cycle has completed. I discharged the battery and let it rest overnight. I then sent "IT ENABLE" command followed by "RESET", per the instructions in SLUA903 section 3.2.1. However, Update Status 0 remained at 02.
I manually changed Update IT Enable and Update Status 0 to 00 in the Data Memory page. I then tried again to send IT ENABLE and RESET commands. IT enable changes to 1, but Update Status 0 stays at 00. (Update Status 1 is also at 00, but I think this does not matter as LU_PROF is set to 0).
What is the correct way to reset the gauge to the point where the learning cycle can be run again? I was expecting RESET to do this, but it doesn't seem to have any effect on Update Status. I did make sure that the device was unsealed before sending RESET.
Any advice is much appreciated.
Thanks,
Dave