This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2663: UVLO connection with reverse polarity FET

Part Number: TPS2663

Section 9.3.3 of the datasheet says: In the applications where reverse
polarity protection is required connect a minimum of 300-kΩ resistor between UVLO and IN_SYS.

What if the desired UVLO operation at 15V is desired, where the UVLO pin is connected to GND?

Is it valid to connect UVLO to GND, when the TPS26631 is configured with external FETs providing reverse polarity protection?

Thanks

Will