This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8556: LP8556SQE-E09 BOOST Output 43V feasibility

Part Number: LP8556

We are using the "LP8556SQE-E09" LED backlight driver on our LED driving board.

We want to use it to drive a light bar configuration that require 43V BOOST Output and 23mA max LED current for each of the 6 channels.

Estimate power: 43V*23mA*6 = 5.93W

According to the datasheet, the "BOOST OUTPUT" range of the IC is 16V to 34.5V:

Questions:

1) If we change the 0x9E and 0xA9 parameters each time during power ON sequence, can we set the BOOST Output  Voltage of the IC to 43V?

2) Will we able to update the EEPROM to set the BOOST Output  Voltage of the IC to 43V?

3) Is the IC capable of driving 6 channels with BOOST Output  Voltage=43V, LED current 23mA/ channel?