Other Parts Discussed in Thread: BQSTUDIO
Hello,
I am currently investigating firmware programming of the BQ27Z561. I have read slua801.pdf and many posts on this forum, and some questions I have not found an answer to are the following:
Question 1: Are all BQ27Z561 IC's pre-programmed with application firmware when manufactured by TI?
Question 2: Assuming the answer to #1 is yes, what happens if production boards are built with newer BQ27Z561 firmware than what the MCU expects? Is a new golden image (battery characterization) needed?
For example, lets say we have 1000 devices with a BQ27Z561 pre-programmed with firmware version 1.00 by TI. A golden image is created in the file format df.fs and programmed to all 1000 devices at application boot as a one time occurrence by me. All 1000 devices are deployed in the field with version 1.00 and golden image data flash.
I then build 1000 more devices, but the preloaded firmware in the BQ27Z561 manufactured by TI is v1.01.
Is a new golden image needed for firmware version 1.01?
Thanks,
Derek