This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92662-Q1: NO RESPONSE FROM UART INTERFACE

Part Number: TPS92662-Q1

I have been tasked to develop MCU firmware and a GUI to interface with this part. My MCU firmware encodes UART RX/TX frames and appends the CRC16 H/L bytes. My problem is that there is no response from my UART messages.

VIN: 12V -> VDD: 5.0V, VIO: 3.3V, and AREF: 2.5V

CLK: 6MHz (Crystal) -> SERIAL BAUD RATE: 375K


INIT: Write Byte (0x87)

DEVID: Serial Address (0x20) [0 0 1 0 0 0 0 0]

REGADDR: Register Address (0x80)

DATA: Data Byte (0xA1)

CRCL: 0x89

CRCH: 0x06

Logic Analyzer capture:

Scope capture:

I have the full datasheet (SLUSCU8 –JUNE 2017) but I don't have the User's Guide or any code examples to verify that I am talking to the part correctly. I have read here that others have also run into this issue, but since none of the responses are published, I have to bug someone with the question again.

Any help would be appreciated.