Hello!
I have a few questions on the BQ24030RHLR:
- If AC > 6V, VOUT is regulated to 6V. I don’t see a description of this. I take it, it is just PWMed so the average voltage = 6V (i.e. id AC=12V, Vout would be a 50% duty cycle, 12V peak). Is this the case?
- If the AC is connected and the charge is complete, this draws <5uA, and the battery is disconnected (AC driving board/OUT). If the AC and USB are disconnected, VBAT is connected to OUT (Q2) and the charger takes <5uA. Right?
- This is 1.5A max charge current, right? Is there a similar chip with 2A or 2.5A charge current?
Thank you!
Sarah