This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: BQ40Z50-r1 CUV

Part Number: BQ40Z50-R1

Hi

I am using a BQ40Z50-r1 4S1P Battery Pack.

In this I have the following queries

1.The CUV set Voltage is 2.75 V per cell. During Discharge when the one cell voltage Reaches 2.75V,The CUV bit is enabled and Charging terminates. After sometime again the battery takes discharge current and then Discharge and Again CUV Sers it cuts off. It does not comes to Complete rest position.

2.During Discharging a err file is created. In that it displays TIMEOUT OR UNEXPECTED ERROR FROM DEVICE for some Certain parameters during logging.

Kindly need some suggestion to resolve the issues.