Dear team,
My customer wants to connect ON pin to VIN pin directly without resistor, is it ok?
Thanks & Best Regards,
Sherry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
My customer wants to connect ON pin to VIN pin directly without resistor, is it ok?
Thanks & Best Regards,
Sherry
Hi Sherry,
Thanks for reaching out on E2E!
It is possible to connect the ON pin to VIN without a resistor between them, however there are some things to consider:
- Rise time will be affected as VIN is changing. Shorting ON to VIN will affect the timing seen and the system will differ from the expected datasheet values.
- EN cannot be left floating which is possible with a loss of Vin. If the device is powered and the ON pin is floating, we cannot confirm if the device is ON or OFF, meaning the device could also be partially ON.
As mentioned in the datasheet, we don't support ON floating. Therefore, we recommend a pull-down resistor from ON to GND to be used.
Best Regards,
Elizabeth
If my reply answered your question, please click the "This resolved my issue" button. This can help others verify that a solution was found!
Hi Elizabeth,
Thanks for your reply!
1. I don't understand why rise time will be impacted if ON connects to VIN directly. Is there the power sequence requirement between these two pins?
2. If ON, VIN and Vbias are connected together, ON pin won't be left floating under powered mode because they turn on/off at the same time. If the device is unpowered, it should be ok that ON is in floating status, right?
Thanks & Best Regards,
Sherry
Hi Sherry,
Allow me to clarify,
Best Regards,
Elizabeth