This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28056: UCC28056 in a 250W LED power module design,questions about THD

Part Number: UCC28056


Dears

based on this question: 

UCC28056: UCC2856 in a 200W pwer module design,when test the half full load and 3/4 full load , is it possible that THD<10% ? - Power management forum - Power management - TI E2E support forums

My  customer also have other questions, please check and support!

UCC28056 (used in  250W and 250W below LED power module):

When input voltage is 110Vac and 230Vac,half load, can the THD<10% ?

When input voltage is input voltage is 277 Vac,75% load, can the THD<10% ?

When the input voltage is 230 Vac and half load, can the power factor reach or greater than 0.95?

Thanks!

  • hello user,

    thanks for your interest in UCC28056.

    It is possible for UCC28056a to achieve 230VAC half load and 277VAC 75% load with <10%ithd. at this condition the controller works at DCM.

    But it is very hard for the controller to achieve <10% at 115VAC input since the controller is working at TM mode., Below <20% is possible.

    with DCM can have a better ithd compare to that working at TM mode for this controller.