Dear:
During the chargering, the battery capacity is up to 98%,the gauge status is full, but if the adapt is always plugged in, the battery capacity can be up to 100%; Question :the battery capacity and the gauge status is not same,can you give me any suggestion or direction?