Part Number: DCP020515D
Hi I found an application note sbaa035b in which it is decsribed how to control the Sync Pin to enable/disable the DC/DC Converter.

I have 3 DCP02 in my circuit and I control it with one transistor. Is this OK?
What if I measure a frequency of ~ 580kHz on the sync pin after switching of the transistor, is the frequency of 580KHz OK?
thanks
Achim Stösser
ADD-DATA