This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65287: What are Vout Min and Max for this device?

Part Number: TPS65287

Hi experts

My customer has an application to generate an adjustable voltage from close to 0V up to 12V. 

1) What are the min and max Vout that can be configured with this device?

2) Is it possible to make the output voltage adjustable with a DAC or adjustable resistor in the feedback path?

Thanks!

Jim B