This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV431A: Inquire of ESD (CDM& MM) data

Part Number: LMV431A


I am creating a part number confirmation for LMV431AIMFX/NOPB for my company.

There are more basic information about ESD (CDM& MM) data of parts are required, but we didn’t get them from my contact sales person.

Please help tell me where I can find information or provide data.

  • Hi William,

    Give me a few days to see if I can find the data for you.

    Ben

  • Hi William,

    The information I found has HBM and MM but no CDM.  From the datasheet, the HBM is 2KV, which is shown below:

    For machine model (MM), the voltage for MM = 200V.

    There is no CDM data from the report because CDM was not a requirement when this part was originally released in 2002. CDM was not required by JEDEC for IC qual back then.

    I hope I have answered your question.  Please let me know if you have other questions and I will be happy to help answer them.

    Ben

  • Dear Ben,

    Thanks for your reply with providing MM data, but in our company, the information of MM and CDM is necessarily if the material approval is to be completed.

    Would you please to ask if there is a corresponding unit that can help with the experiment or verify the CDM information?

    In addition, since the information we are asking for is to used for material approval, would you please to provide a complete data sheet including MM and CDM?

    If your company has any difficulties with the information we asked or how long it takes to complete,please reply to the message first.

    Thanks a lot.

    sincerely

    William

  • Hi William,

    I noticed that you are currently working with TI local sales and FAE people.  Since you have been in contact through them, I can work with them to provide the necessary support for your application needs.  If you don't mind, please close the thread by clicking on "resolved" and I will have the local sales and FAE representative reach out to you.

    Ben  

  • Dear Ben

    sorry for my late reply,

    That's OK, I will keep connect with TI local sales and FAE people,

    Thanks for your help.

    William

  • Hi William,

    Thank you and good luck to you!

    Ben