Other Parts Discussed in Thread: BQ76952, BQ76942, BQSTUDIO
I found an error in slua991a.pdf "Easy Configuration of BQ76942, BQ76952 Battery Monitors", "3 GG File Example", Page 11.
The instruction is to select Export->Export Defaults but the GG file listed below is in the form of an Export->Export command.
I used Export->Export, edited, and Import->Import from a file worked without issue. I don't know if the pdf document or the behaviour of BQStudio selections is "reversed" I suspect the document.
But it raised the question of what to use when I am Importing gg files during development. I want to adjust settings and reload the gg after each reset or power cycle rather than use the OTP which I am warned has limited cycles. Aside question, does limited mean it can only blow fuse bits or that it is EE with limited erasures ?
So my main question is, should I be progressively exporting/importing Export Default files or just the Export files as I do development ?
If I use the simpler Export files, what could I change that will be lost (not re-imported) if I am not using Export Default files ?
If this is already documented, I apologise, the learning hill is still a steep climb atm :-)
All the best
Harry