Part Number: LM25184
Other Parts Discussed in Thread: LM25148, , TPS54308
Hi
Can LM25148 be used as isolated power supply POL, DC 5V to DC 3.3V 3A?
There are other recommended products that are suitable
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The input range of LM25184 is 4.5 V to 42 V which might not fit your applications as the 5V might not be so stable.
I have transferred your need to mid-Vin product line.
Regards,
Xiaoying
Hi ,
You can try flybuck solution with TPS54308.
App note as below:
BRs,
Young