This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28600-Q1: Does our device support Single current closed loop control?

Part Number: UCC28600-Q1
Other Parts Discussed in Thread: UCC28740, UCC28600

Dear team,

 My customer uses our device in below architecture to replace UCC28740, but now they encounter one problem. When they are doing current closed-loop control, there will be oscillations. We saw the description in one document 'When the duty cycle of the current mode control converter exceeds 50%, the converter will oscillate at the sub-harmonic frequency of the switching frequency''. We are not sure whether this is the root cause. If it is, do we have any method to avoid the oscillation? Can we limit the duty cycle below 50%? Does our device support Single current closed loop control?

PMP21959RevA_Sch_20190402.pdf

Thanks & Best Regards,

Sherry