Hello,
I have a design where I am using the REF1941 (REF1941AIDDCT) to provide a voltage reference to a set of thermistors (five in total). VREF (4.096V) provides the thermistor rail, and VBIAS (2.048V) is used as an ADC reference.
The datasheet states that the maximum stable output capacitor range is 10uF. The issue is that the thermistors are at the end of a ~2m long cable so the VREF output has to travel down this. Up to now there have been no issues, however some units are potentially now experiencing instability on the VREF output, although this has been difficult to observe on an oscilloscope as the issue seems intermittent (common noise across all thermistor channels).
Do you think the REF1941 is capable of reliably driving down this cable or should additional precautions be taken at the device's output to compensate for this type of load?
Kind regards,
Stephen