The SR IDE function is used in Automatic Mode Switching With Hysteresis.
SR on time is fixed in Auto Config High.
Why the SR_VDS1/2 are need to be sense, and convert to SRDET1/2
What functions are SRDET1/2 and can I disable SRDET1/2?
.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Two ways can fix SR on-time. (1)SRVDS sense, (2) Auto Config High
Which way is used in LLCHBFirmware-1.2?
And how can I modify it to another function?
In LLCHBFirmware-1.2 , SRVDS is not implemented, but it uses Auto Config High to set up max SR on-time.
Again, although the signals are connected, but this feature is not implemented for SR body diode sensing. For SR on-time auto tuning, you should look at UCD3138A + UCD7138 chip set.