This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25171-Q1: Charger IC solution of NiMH charging Request

Part Number: BQ25171-Q1
Other Parts Discussed in Thread: BQ24400, BQ2002T, BQ24105

Hi Team,

My customer has a NiMH Battery Charging requirement on NAS application.

The NiMH Battery is 3S1P. 

Power Capacity of AA Battery: 3S1P: 2200mAh /3.6V

Charger Temperature at 50C

Customer is surveying related solution and have some questions as below. 

  1. How to reach different battery Inside resistance balance in charging? or need other Charging IC could achieve. Let me know have some choice.
  2. If there are 2 fully charged batteries + 1 dead battery series in system, what is the charger's behavior?
  3. Have other suggestion solution with I2C or SPI also easy to use and low cost
  4. If no need Host control,  Have other good choice that easy to use and low cost?
  5. Do we have other smart battery feature solution can introduce to customer?

Best regards,

Hardy