Other Parts Discussed in Thread: TPS61251, ADS1260
Hello,
I am looking for low-dropout regulators (LDOs) to reduce switch-mode power supply ripple by TPS61251 Boost Converter with typical operating frequency: 3.5 MHz
It is the application in voltage rail for high-precision ADCs such as ADS1260.
The input voltage is +5.5V and the output voltage is +5V.
Here are the questions:
- Which is the most important feature in the datasheet should I concern? (PSRR, Output Range, … etc.)
- I chose TPS7A47x because of the high PSRR at 3.5MHz. Is TPS7A470x ideal choose or other suggestion?

-Jax