This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DC-DC buck converter IC recommended

Other Parts Discussed in Thread: TPS62026, TPS62840

Hi

Based on our requirement, I need a DC-DC buck converter IC to generate 3.3V output voltage for supporting our device power rail. But the input voltage of the DC-DC buck converter IC connects the battery, and the cut-off voltage of our system is 3.3V. I searched the TPS62026 on the TI website. I am wondering if the DC-DC buck converter "TPS62026" is able to generate the 3.3V output voltage when the input voltage of the DC-DC buck converter is 3.3V? I am not sure whether the TPS62026 can meet my requirement. If not, may you help provide the recommended DC-DC buck converter? Thanks.

Derek