Other Parts Discussed in Thread: TPS25750, BQ25790, BQ25792
Hi,
I am familiarising the USB-PD-CHG-EVM-01. I connected 2 Series Li-ion batteries and flashed a configuration bin file generated by "TPS25750 Application Customizaion Tool Version 7.0.1.3" into the EEPROM. When I connected Samsung's adaptive fast charging adapter (EP-TA200) and Samsung's PPS supported Super fast charging adapter (EP-TA800) to the Type C receptacle, I observed that instead of charging the battery, the EVM is drawing a current of 30mA from the battery. No load is connected to the VSYS (J1). What might be the issue?
Configuration which is used to generate the bin file
1. Select your configuration:
- power source (provider) and a power sink (consumer) top-left config. (Default one)
2. What is the maximum power that can be sourced?
- 15W (5V)
3. What is the required sink power or power consumed?
- 100W (20V)
4. What is the preferred power role?
- Power sink (consumer)
5. Do you have a preferred data role?
- No
6. What is the supported USB Highest Speed?
- No USB data is being used
7. Do you have a Vendor ID provided by the USB-IF?
- No, use the TI Vendor ID in the Vendor Information File (VIF)
8. Do you have a desired Product ID?
- No, use "0x0000" as the Product ID
9. Select the battery charger component to integrate:
- BQ25790 or BQ25792
10. What is the battery charging voltage?
- 8.4V
11. What is the battery charging current?
- 500mA
12. What is the charge termination current?
- 80mA
13. What is the pre-charge current?
- 40mA
Some observations:
- TP1 (PPHV) readings were:
- 9V when EP-TA800 adapter was used.
- 5V when EP-TA200 was used.
- MODE register of the PD controller was read to be "APP<SP>"
- STATUS LED (D1) was also ON during that time.
- The VSYS voltage was fluctuating between 1.9V and 2.3V when the battery was disconnected. When the battery was connected, the voltage at VSYS was seen to be the same as of the connected battery.