This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51116: S3, S5 pins connection

Part Number: TPS51116


Hi!

I'm using TPS51116 in my design for DDR4 power supply.

Can I connect S3,S5 pins just to PGOOD output of another DC/DC converter? I mean our SoC (LS1028A) doesn't have special outputs for managing S3,S5 inputs of TPS51116 for sleep mode.

 

Thank you!

Sergej.

  • Hi Sergej,

    As long as the below behavior works for your system then it's ok to connect S3/D5 to PGOOD output of another DC/DC converter:

    1. When both S3 and S5 are high, VDDQ/VTT/VTTREF outputs are high

    2. When both S3 and S5 are low, VDDQ/VTT/VTTREF outputs are low. 

    Regards,

    Weidong