Hi,
I'm looking at using the TPS62913 in a design that requires 11-13V input to 3.3V output @ 3A.
I read in the datasheet that it suggests that for best efficiency a 2.2uH inductor can be used so long as Dmax is under 45%. However, when I create a custom inductor in Webench of 2.2uH, it warns me that the recommended minimum value is 3.3uH.
Where does webench generate its minimum recommended value from and should I be concerned about this?
Also, can you clarify what the issue is, if the inductor is too small - e.g. 1uH for instance?
Many thanks