This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55340: Heating Issue

Part Number: TPS55340
Other Parts Discussed in Thread: LM5155

Dear Sir,

              I have designed TPS55340 Based BOOST Converter with Vin as 12V and Vout as 35V with a switching frequency of 600kHz. I found that IC was getting heated up when I tried to draw 1A output. Is there any means to resolve the heating issue or is there any design improvement or design flaw that I have done ?. Kindly guide me on the above scenario. My actual requirement is to charge an 8S Li-ion battery with a 12V charger. Hence I have to boost 35V and charge at 1.5A. Kindly suggest if any other alternate solution is available.

Thanks & Regards,

Praveen Kumar G