This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZM23601: Power Rail for PGOOD Pull-up Resistor

Part Number: LMZM23601
Other Parts Discussed in Thread: PSPICE-FOR-TI

Hi,

I'm designing a step-down converter using LMZM23601 part. The anticipated input voltage applied to VIN pin is +5V and the output voltage of the converter is +3.3V. A 10K Ohm pull-up resistor on PGOOD pin will be connected to the separate independent +12V dc power rail. Although this value seems to be within Absolute Maximum limits for PGOOD pin that allows +16V max, I still have a concern regarding this voltage being higher than VIN input power.

Q1: Is it OK to use PGOOD pull-up voltage rail higher than VIN?

Q2: I tried to simulate this situation using PSpice-for-TI software and noticed that PGOOD never raises above VIN. Does it mean that there is a clamping diode between PGOOD and VIN pins or some other voltage-limiting circuit that limits the PGOOD voltage?

Please clarify this situation for me.

Regards,
Michael