This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31506: About PWRGD terminal specifications of LMZ31506RUQR

Part Number: LMZ31506


Could you tell us about the PWRGD terminal specifications of the LMZ31506RUQR?

There is a description of the TYP value for the PWRGD threshold, but there is no description of the Max value and Min value.

Could you tell me about the value?

  • Hello,

    The power good pin does not have a min or max spec for this device. The typical specification will provide the percentage thresholds at which power good will assert and de-assert. For example, when Vout rises and achieves 94% of the set point, PG will assert high. If VOUT rises to 109% of the VOUT set point, PG will de-assert. For VOUT falling (from above the set point), PG will assert high when the output voltage falls to 106% of the set point. As VOUT decreases further, PG will de-assert when VOUT falls below 91% of the set point. 

    Sincerely,

    Alec Biesterfeld