Hello,
I have a question about I2C rise /fall time measurement.
I searched past questions, the rise/fall time of I2C was 10% -90%.
Please see the waveform below.
It can be seen that the L voltage is 0.27 V, but since the VIL is max. 0.4 V, I think there is no problem.
In this case, since the Tr time cannot be measured from 0.18 V of 10%, is it correct to assume that it is a time from 0.27 V to 1.62 V of 90% as in this waveform?
Best Regards,
Hyodo