Other Parts Discussed in Thread: TPS63070
Due to supply issues with the TPS63070 we are trying to re-arrange an existing product to use an existing onboard TPS76301DBVT. Its rated at 150mA continuous. Our circuit draws a peak current of about 180mA for 50mS per second at 3.8V voltage output but the rest of the time is <5mA. Input voltage is 5.2 - 6.4V.
Are we OK to use like this? We can't damage the device as its current limited (at about 0.8A). The graphs on P7 of datasheet shows a slight reduction of output voltage at 180mA.
We have tested it and it seems fine but its a bit unclear from the data sheet.
Thanks in advance
Liam