Part Number: USB-PD-CHG-EVM-01
Other Parts Discussed in Thread: TPS54531, BQ25792, TPS25750,
Hi,
when reading the design guide, I found various references to the 5V source in OTG / PD mode.
For the buck converter TPS54531 it is described that this serves as 5V source and only the higher voltages come via PPHV from the charger BQ25792. (Only?) for a Sink-Only application, this device is not needed.
On Figure 3-1 "TPS25750 Application Selection" I cannot find a selection for different sources via PP5V and PPHV.
On Figure 3-9 "Sourcing 5 V with BQ25792 in OTG Mode" and following text it is described that the BQ25792 generates the 5V.
How does the USB-PD-CHG-EVM-01 really work in standard configuration?
How can I configure different sources using the Application Customization Tool? 5V via PP5V and higher voltages via PPHV
As far as I understand, the 5V converter TPS54531 is only needed for higher output currents >3A. Up to 3A, the BQ25792 can also be used as 5V source. This should be the "BQ only selection" in the Application Customization Tool. Is that true?
Regards,
Achim