Used +15v to 5v, device latch up automatically. Sometimes it is recovering. Sometimes not recovered.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Used +15v to 5v, device latch up automatically. Sometimes it is recovering. Sometimes not recovered.
Hello Karunakaran,
Can you explain more about the issue or problem you are having?
When you say "latch up" are you referring to the input voltage, output voltage, or a different pin?
Thanks,
Joseph
Karunakaran,
What conditions is the output voltage going to zero, Are you testing at no-load, full-load? Is there a possibility that the system is short-circuited?
Do you have a schematic of the setup? This will help further solve the issue.
Thanks,
Joseph
At No load condition itself it is going to zero volt
Can I have your mail ID to send sch
Initial stages powered ON, and working good for both load and no load condition, 2-3 days worked good. after that it got failed during power cycle. same is happened for 2 boards.
for sure there is no input spikes, because am using precision power source with 6 digit accuracy. Some thing else got problem in IC/Design