For the BQ7791500 to recover from UV fault, does it absolutely need to detect load removal?
In the datasheet, "9.3.2.2 Operation in UV" section, it seems to indicate it can recover after a delay without load removal:
9.3.2.2 Operation in UV
A UV fault detection is when at least one of the cell voltages is measured below the UV threshold, VUV, for a duration of a UV delay, tUVn_DELAY. The DSG FET is turned off.
The UV fault recovers when:
• The voltage of the cell in fault goes above the (UV threshold + UV hysteresis, VHYS_UV) for a time of a UV delay OR
• The voltage of the cell in fault goes above the (UV threshold + UV hysteresis, VHYS_UV) for a time of a UV delay and the load is removed.
We intend to use the BQ7791500 in a device where the user cannot remove the pack. We could 'fake' a removal by briefly grounding LD, but would rather not.
Thanks!