This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92682-Q1: Low frequency oscillations under light load

Part Number: TPS92682-Q1


Could you please help to confirm if the Drain voltage oscillations on the MosFet as below is because of TPS92682-Q1 work under DCM mode under light load? If it is because it work under DCM mode, then could you please kindly help to share some theory analysis about why there would has the low frequency oscillations here? Since currently, my customer need to provide relate test result to OEM but they could not explain the reason why the waveform look like following picture shows, thank you very much for your support .

Red: Vdrian to ground(MosFET)  Yellow: Vgate to ground.

Best regards

Jie