This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61165: Fig.16 External PWM Dimming Network

Part Number: TPS61165

Hi team,

I have a question about the Fig.16 circuit. I think that this circuit is for analog dimming from PWM signals that are below 5 kHz. If customer has 5k to 100kHz PWM, they can use Fig.8 circuit. Is my understanding correct?

Also, Fig.16 states that "Drive Three High-Brightness LEDs". If customer wants to drive the LEDs with High-Brightness(High current), should customer use the Fig.16 circuit? If so, could you tell me the standard(threshold) of the LED current(mA)? For example, if the ILED is more than 300mA, Fig.16(External PWM Dimming Network) is recommended.

Regards,

Yamaguchi

  • Hi Yamaguchi-san,

    Fig.16 is a way to achieve PWM dimming and the frequency cannot be too high, since there need some time for loop stability. PWM dimming or analog dimming is for output side. PWM dimming means changing output duty cycle to adjust output current, while analog dimming means changing peak current level. The inputs are all PWM signal. I think the decision of choosing PWM dimming or analog dimming is decided by whole system requirements, but not the current setting.

    For ILED range, it is determined by VIN and VOUT. Assuming the efficiency is 90% and there are 100mA current ripple on inductor. Since the current limitation of internal switch FET is 1.2A, the max output current is around VIN*(1.2A-0.1A) * 90% / VOUT.

  • Hi Hardy-san,

    Thank you for the answer. Please let me check my understanding just in case. 

    The Fig.16 in the TPS61165 d/s is analog dimming. Is it correct? Please see the Fig.1 in the app note below. 

    https://www.ti.com/lit/an/slva471/slva471.pdf

    Regards,

    Yamaguchi

  • Hi Yamaguchi-san,

    Yes it is still analog dimming. I make a mistake before. This structure used RC filter to adjust the voltage at cathode of LED string.