Other Parts Discussed in Thread: BQ25731
Hi
As a buck-boost charger, we should use 4 mos. 2That id 2 mos before L as buck charger function(Q1/Q2), and 2 Mos after L as boost charger(Q3/Q4).Q1/Q3 highside,Q2/Q4 low side.
My application only use bq25703A as buck mode charger with input voltage 18-20V and 3s Lion battery which highest volatge is 13.2V. Can I only use 2 buck-mode mos before L. So it cost fewer space,and I can use larger mos footprint to improve the heat performance. Meanwhile I still use the NVDC architecture to supply the system.
Thanks