When I turn on the FET by using FET_EN it doesn't turn on the FETs (erratic behavior). But if I use DSG_FET_toggle and CHG_FET_Toggle it turns on. Also while charging the pack at 3A after few minutes the Fets turn off with CTOS flag set.The CTO threshold is 2500mA, I wanted to know if this value needs to be set more than the charging max current? But I had not experienced the same behavior earlier without making any changes to CTO parameters.
This is the wave form across gate and source of discharge FET,when enabled using FET_enable.The only difference between FET_enable and DSG_Toggle is that in FET_EN enables both CHG_FET and DSG_FET are turned on simultaneously.
\
This is when DSG_Toggle was used.